Program
   BeforeStart
     Move to Initial start position
       MoveJ
         'CAUTION: check reachability or edit Waypoint before running Demo!'
         Start
     FT Sensor: Enabled
     'Initialize variable for use in thread'
     ATI_FT_rawdata≔ati_ftsensor.get_raw_ft()
   Robot Program
     Bias the sensor
       Wait: 0.5
       FT Sensor: Bias
       Wait: 0.5
     'This Demo program shows multiple ways to read F/T data for a "Force Search" in Z direction'
     METHOD 1: Read F/T data via native UR command
       MoveL
         'Move down until the tool touches a surface'
         If force()<2
           RelativeMotionZ
         'Wait, then return to the start position'
         Wait: 1.0
         Start
     METHOD 2: Read raw F/T data via ATI F/T URCap command
       MoveL
         'Move down until the tool touches a surface'
         If ATI_FT_Fz>-2
           RelativeMotionZ
         'Wait, then return to the start position'
         Wait: 1.0
         Start
   Thread_1
     'MONITOR THIS DATA DURING PROGRAM FROM "Variables" TAB'
     Wait: 0.01
     'Read sensor F/T Data using F/T URCap command, & assign it to a variable.'
     'This is the raw data directly from the sensor, in the sensor coordinate frame.'
     'With every loop of the thread, update the raw F/T data reading.'
     ATI_FT_rawdata≔ati_ftsensor.get_raw_ft()
     'Fz is the 3rd element of the ATI_FT_data variable.'
     'NOTE: Pressing sensor in Z causes a -Z force (if no sensor Tool Transform applied)'
     ATI_FT_Fz≔ATI_FT_rawdata[2]
     'F/T sensor data can also be read from native UR commands.'
     'Data read from UR commands will have transformations applied.'
     '(it is in robot base frame, not in the sensor coordinate frame).'
     ' UR Command get_tcp_force() gives TCP force in coordinate frame of robot base.'
     FTinBaseFrame≔get_tcp_force()
     'UR command force() gives the Norm of get_tcp_force().'
     ForceNorm≔force()